cancel
Showing results for 
Search instead for 
Did you mean: 

STM3241G Eval board SDIO 4-bit wide access issue.

Posted on June 11, 2018 at 17:37

STM3241G Evaluation board: unable to access SD card with SDIO 4-bit wide bus configuration and with SDIO DMA access for both 1-bit & 4-bit wide bus. Attempt to access SD card will always results in timeout error. 

Also i

nitialization code generated from STM32CubeMx for toolchain TrueStudio will always have 1-bit wide definition even when SDIO 4-bit wide is configured.

#stm3241g-eval-board-sdio-4-bit-wide-access-issue.
1 REPLY 1

Use the examples under the HAL/Cube tree, should be some specifically for the EVAL board, along with others that could be ported.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..