2012-04-25 1:39 AM
I am new to and using the Stm3240g Board Firmware.
I have a problem with the Ports though. With the Usb and SDCard enabled (nothing else attached), I can Enable Port PA and PB. But when I enable Port PE - then PA and PB become nonfunctional, while PE still seems not working either. Does this make sense ? (At the same time, Port PD seems to be running as a Timer.) I am simply toggling Pins once per second. Enabling PE is enough to cause the problem. Any Ideas ? Is there a conflict in how I enable Ports - or a Stm3240g Problem ?