2014-10-15 3:49 AM
Hi,
I have downloaded uC/TCP-IP stack from Micrium website and I am using STM3210C-EVAL board. I am running the example code of DHCP client given by micrium on this board but the Ethernet is not working properly. I have found on the micrium website that the uC/TCP-IP stack is for the board uC/STM32F107 (part No. BRD-EVAL-STF107-P-P1). I wonder why it is not working as the micro controllers are same on both the board. Is there any different between two Eval boards? How I can run the TCP/IP stacke of micrium on the STM3210C-EVAL board? Regards, Gunjan #uc/os-iii2014-10-15 4:19 AM
I guess you'd start by reviewing the schematics, checking the PHY used in each design and the pins and clocks, and make sure you've suitably ported the code to address any differences.