Associate
November 24, 2020
Solved
STM32 working with impulsive magnetic field condition. Something to take care?
- November 24, 2020
- 2 replies
- 5187 views
Hi all, I have an application under test with MCU STM32F411 that working in impulsive high magnetic field generate by a big inductor. Below the specification:
- duration of impulse 400us;
- intensitiy of magnetic field is 2,5 Tesla peak;
- magnetic filed has a shape of sine wave with 400us duration that is 1 cycles.
- repetition of impulse is in range of 1Hz to 150Hz repetition (1s to 6ms).
- pcb with MCU and EEPROM are apply over coils at 1cm distance
I would like to know if these conditions are dangerous for STM32F411 its internal flash source code application or SRAM data that may be currupt by magnetic field.
Any suggestion to keep control internal MCU or SRAM content that can be currupt by impulsive high magneti field?