Hi Gael,The FMC always samples the data before deasserting the Chip Select signal, that's to make sure that the data is read before deselecting the memory which may abort outputting the data from the memory side.The data setup time is about to give e...
Hi Vins,You're not using STM32F769I discovery or eval kit ? maybe check the screen configuration.is other demo or application running smoothly ?Regards,MHaj.
Hello,Here my thoughts on this, the difference in behavior between F4 and L4 is in the option bytes programming, in the L4 Setting OBL_LAUNCH generates a reset (RM0351 page 117) while the F4 option byte programming does not require (RM0386 page89), I...
What are the pins used for the ADC read ? I gave the attached photo an extra look and the PA1 isn't connected, same for PA12. If the ADC pin is close to those unconnected pins maybe a change in their GPIO config may help, also maybe adding protection...