2008-03-25 9:10 AM
STM32 virtual com port sample in Vista?
2011-05-17 3:25 AM
Does STM32 virtual com port sample code test in Microsoft Vista OS?
2011-05-17 3:25 AM
I understand that Windows Vista64 already completely prevents use of unsigned drivers.
It would be good if ST could kindly provide STM32 users with a ‘signed’ USB CDC Virtual com port driver (rather than an unsigned driver), because Microsofts intention is to ‘reduce the number of unsigned drivers in the field’. For ST's virtual com port example, download;- STM32F10xxx USB developer kit from and look in folder: STM32F10xUSBLib\\USBLib\\demos\\Virtual_COM_Port [ This message was edited by: bobz on 20-03-2008 18:25 ]2011-05-17 3:25 AM
> I understand that Windows Vista64 already completely prevents use of unsigned drivers.
take a look here:http://www.start64.com/index.php?option=com_content&task=view&id=1200&Itemid=73
but microsoft is vomit:http://www.linchpinlabs.com/resources/atsiv/usage-design.htm