2015-08-14 6:33 AM
Hello Guys,
My product can not send data to my computer since I upgraded it from Windows 8 to Windows 10.So I have one question, meanwhile a new version of the driver is released, how can I fix this issue ? Thank you per advance for your support.ZBH #!stm32-!vcp-!windows10-!driver2018-11-17 12:08 PM
I have Windows 10 and cannot get the MKI109V3 to work. The computer will not communicate with the board. The COM port will not open. The UNICO-included drivers are not compatible with Windows 10. I have dutifully followed all instructions included with the devices, however, as mentioned previously, the drivers do not seem to be compatible with Windows 10.
I am not computer literate, I'm simply trying to help my son do a high school science project on bike helmet safety, and this is the only system MKI109V3 with MKI153V1 that will measure the G-forces he needs.
I'm open to any and all suggestions.
Best -- David
2018-11-17 12:30 PM
You might want to start a new thread in the sensor forum, it's going to get little traction in a 3 year old thread
https://community.st.com/s/topic/0TO0X000000BSqTWAW/mems-and-sensors
2018-11-17 12:39 PM
David,
Why do you think that the supplied driver is not compatible with Windows 10? Is there any error message? Of course, without a proper driver on Win10 side the board cannot talk to the PC. Try to find someone computer literate to check what is the issue with the included COM port driver, and whether it can work with Win10 own driver instead.
In my experience, Win10 has USB-CDC driver that works with STM32.
-- pa
2018-11-18 7:56 AM