cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 VCP vs Windows 10

zaid23
Associate II
Posted on August 14, 2015 at 15:33

Hello Guys,

My product can not send data to my computer since I upgraded it from Windows 8 to Windows 10.

So I have one question, meanwhile a new version of the driver is released, how can I fix this issue ? 

Thank you per advance for your support.

ZBH

#!stm32-!vcp-!windows10-!driver
This discussion is locked. Please start a new topic to ask your question.
13 REPLIES 13
Posted on August 14, 2015 at 16:42

And this is why it's important not to rush into upgrades where the vendors of your critical components aren't chasing Microsoft's latest tangent.

Aren't the WHQL tests supposed to prevent these types of issues? What has Microsoft changed that has broken the ecosystem?
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
zaid23
Associate II
Posted on August 17, 2015 at 10:52

Hello Syrine,

Thank you for your quick feedback.

In fact, I have one customer among forty who is not facing the issue. Can someone let me know which files are installed and where they are installed by the VCP install tool ? 

I want to check if it is not due to a change of the address of the folder.

Thank you for your feedback.

Nesrine M_O
Lead II
Posted on August 17, 2015 at 12:47

Hi ZBH,

 

It should be under C:\Program Files (x86)\STMicroelectronics\Software\Virtual comport driver

-Syrine-

zaid23
Associate II
Posted on August 25, 2015 at 08:49

Hi Syrine,

I have checked with a customer on his 2 computers, one powered by Windows 10 Pro, the second by Windows 10 Home.

My product with my software made with the STM32 VCP driver is only working with the Home version.

I can not understand the difference of the install of the driver on both operating systems and why this difference.

Does anyone have a clue for helping me to solve this issue ? 

B.R.

LMI2
Lead
Posted on August 26, 2015 at 01:02

Perhaps there are differences how different W10 version get their drivers. Like download from MS update or not. Have you looked at some Window 10 forums, there are several of them.

zaid23
Associate II
Posted on August 27, 2015 at 14:03

Hi Mich,

Yes I did : 

http://blogs.msdn.com/b/usbcoreblog/archive/2015/07/29/what-is-new-with-serial-in-windows-10.aspx

https://msdn.microsoft.com/en-us/library/windows/hardware/dn707976(v=vs.85).aspx

''In Windows 10, a new INF, Usbser.inf, has been added to %Systemroot%\Inf that loads Usbser.sys as the function device object (FDO) in the device stack. If your device belongs to the Communications and CDC Control device class, Usbser.sys is loaded automatically. The driver is loaded based on a compatible ID match similar to 

https://msdn.microsoft.com/en-us/library/windows/hardware/ff538820%28v=vs.85%29.aspx

.''

I am not a specialist but I think the driver got to be updated. Am I wrong ? 

In the README file released with the driver I can read ''Supported OS : Windows XP to 8.X''. There is not ''Windows 10'' on it.

Thank you for your support. The issue starts to be very critical for me.

B.R.

Zaïd

chintu_kailash
Associate
Posted on June 22, 2016 at 21:54

Hello ZBH,

I'm facing the same problem on my Windows 10 right now. The post is couple of months old and am assuming you found a solution. Do you mind sharing with me please?

markpdbailey
Associate
Posted on August 22, 2016 at 12:52

The driver files will be installed at 

C:\Program Files (x86)\STMicroelectronics\Software\Virtual comport driver\Win8

Open a command prompt and cd into into this directory

run

dpintst_amd64 /LM

Click yes on the driver installation boxes