cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 USB VCP problem under Windows 10

Bence Stocker
Associate II
Posted on November 14, 2017 at 01:25

Hi,

i use STM32F107RB in my project wherein is an USB VCP virtual com port driver (The basic of the USB VCP is the STM3210C-EVAL_USB_decice_VCP example of the Atollic True Studio). It works well if i use under Windows 7 or Windows 8. But it doesn't works under Windows 10. I tred to update the USB driver on Windows but it didn't solve the problem.

Does anybody have any solution?

Thanks!

0 REPLIES 0