cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 USB Communication ISSUE(communication device class)

dspark
Associate II
Posted on July 11, 2016 at 07:46

Hello,

I have some problem to USB communication.

Hello,

I have some problem to USB communication.

when I tested USB communication device class, my computer was shutdown and reboot.

so I checked the dump memory, but I don't know what this means.

I think this is not the hardware issue or PC application.

because I replace the PC, target Boards(STM32F4Discovery) even replace the MCU(STM32F103).

but when I uses 8051 and UART bridge, it works well.

so I suspects the firmware or usb driver.

please review my problem.

--------------------------------------------------------------------------------------------------------------

Test Environment

Target Board: STM32F4Discovery

0690X0000060MnTQAU.gif

0 REPLIES 0