cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F446 FOC Motor Library 4.2 Compatibility

steve239955_stm1
Associate
Posted on May 07, 2016 at 06:51

Hello everyone,

I was hoping to use this microcontroller with the ST Motor Control Workbench and associated FOC 4.2 library. It seems from the RN0085, that the STM32F446 family is not supported. The strange part is, the evaluation clearly has the motor controller interface connections and the ST Motor control workbench is configured based upon STM32Fxx devices. 

I've already created a board and would rather not downscale to the F405 series or similar devices, as I will need to modify the hardware. I chose the F446 because of the 4 SPI peripherals that I needed in the application. 

From the F446 datasheet, it seems that it is software compatible with some other devices, so can I just 'pretend' I am using the F405? What about if I try to use the 4th SPI peripheral in that case?

any insight would be much appreciated - 

Stephen

#stm32f446-foc-motor-bldc
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
steve239955_stm1
Associate
Posted on June 06, 2016 at 08:23

Nobody knows? 

Does ST's engineering team support this forum, or is it purely users?

valentin
Senior
Posted on June 07, 2016 at 04:44

I've seen ST around here.

Maybe try with a more descriptive thread title?

sbir711
Associate
Posted on July 11, 2016 at 05:37

I'm interested in this as well. Hopefully ST can give a useful answer...