2018-08-10 11:03 AM
Hello! I have a problem with half-duplex in USART. I connected two boards in this mode. Gpio
mode is open drain in each boards.
In the first case I use internal pullup resistor. The transmission doesn't work.
In the second case I use external pullup resister. The transmission works.
could you explain Why ?
2018-08-10 11:18 AM
Some random external resistor value, or something specific? Which STM32 part?
Nominally they are 30-50K on the datasheet of the part I looked at (STM32H7), very low wattage.
2018-08-10 11:34 AM
External resistor is 10K.
STM32F091CC and STM32F417 are connected.
2018-08-10 11:48 AM
More importantly, what baud rate? At higher baud rates (>= 115K) even 10K may be marginal. The issue is rise times when the open-drain releases. Depends on board capacitance, etc. The smaller the pull-up value, the faster the rise time and the higher the baud rate you can handle. Look on a scope if you have one and check rise time vs. bit period.
2018-08-10 12:45 PM
Baud rate is 115200bps.
2018-08-11 6:05 AM
Bob S thank you for help. You are right. The problem was in the connector between boards. It has a big capacitance and the rise time is slow.