cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 STLINK Detect problem

Operi.1
Associate II

0693W00000DlwLNQAZ.jpgHello

I am using stm32f072c8t6 in my project but stlink does not connect stm32 somehow

How can I detect the fault?

boot pin > 10k > GND

NRST pin>10k 3.3v

4 REPLIES 4

Make sure the board is properly powered, and the VTarget pins 1 or 2 on the 20-pin ST-LINK header are connected to the 3.3V of the board

Double check the part orientation, and that you've correctly identified pin 1

Show a picture of board with ST-LINK attached to it.

Schematic looks Ok, check the voltages on the board.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Operi.1
Associate II

0693W00000DlwRLQAZ.jpg0693W00000DlwRGQAZ.jpg

Need to connect the 3.3V pin to Pin 1 on the ST-LINK 20-pin connector (bottom left as pictured)

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Operi.1
Associate II

that cable was connected normally and it came out while taking pictures.

bidet gives internal command error in keilde debug section