2016-06-14 11:26 PM
Hi,
In STM32F105xx datasheet, in part numbering section, it has an option named ''Software option'', and it has two options: internal code or black. What does it mean? #!stm32 #part-numbering2016-06-15 12:04 AM
Factory programs customer supplied firmware in flash during final test procedure?
2016-06-15 08:07 AM
You mean for example in mass production they give the compiled code to factory to program the microcontrollers?
2016-06-15 08:26 AM
Yes, if I were making a million dishwashers, and I just wanted to build boards and plug them in and go without having go through a 30-90 second programming process on each one or expose debug/programming headers.
ST has also had STM32 parts supporting JAVA, these come preprogrammed, not sure if that uses FLASH or ROM