cancel
Showing results for 
Search instead for 
Did you mean: 

Limitation with Read protection active with stm32f105rb

Marco1
Associate II
Posted on June 15, 2016 at 16:03

Hi, 

I made a loader with usb STM32F105 and working properly. When I active the read protection bit, the loader not erase the pages. The security bit is on and of course, I can not debug and find where is the problem. There are limitations on access to the internal flash with the read protection active ?

The write protection is disabled for all sectors.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Marco1
Associate II
Posted on June 15, 2016 at 17:09

I found the answer....

â—� pages 0-1 (for high-density and connectivity line devices) are automatically write-protected. The rest of the memory can be programmed by the code executed from the main Flash memory (for IAP, constant storage, etc.), but it is protected against write/erase (but not against mass erase) in debug mode or when booting from the embedded SRAM.

Can i remove (via software) write protection from page 0 and 1 or its impossible ?