cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 OV7670 DCMI

Marcomech
Associate

Hello, for a few days I have been trying to run the OV7670 camera on the STM32F446RE (Nucleo).
Since the full QVGA RGB565 (153600 B) does not fit in RAM, for now i opted for QVGA Y8 Grayscale, however i must have some problem with how im configuring something  because i cant see anithing from the image in UART terminal and using the debugger im only seeing '00' in the buffer.
Feel free to ask if you need further context or files. 

Regards, Marco

0 REPLIES 0