cancel
Showing results for 
Search instead for 
Did you mean: 

STM32-MAT TARGET work with matlab2019a error:" Reference to non-existent field 'codeFormat'."

Kg
Associate

I use the STM32demo /PIL/"Filter" with the matlab 2019a, Then , I get the next information 0690X000008j9RRQAY.png

And when I used the matlab 2018b, there are some others errors"invalid index"", if the STM32-MAT target is older ? so which matlab version is best matching?

@Amel NASRI @PascalR

1 REPLY 1
Cyril FENARD
ST Employee

​Hi,

This problem is solved with the version 5.1.0 of STM32-MAT/TARGET, published end of July 2019.

Regards.

Cyril