cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 L412 Timer interrupt not working

SSaiy.1
Associate III

I am using STM32L412 microcontroller and doing baremetal programming for timer interrupt. I am using Timer 6 and base clock of 4MHZ is used as HCLK. However my interrupt is not firing below mentioning my code. count variable is also not updating

int main(void)

{

LedConfig();

StartTimer6();

  /* Loop forever */

while(1)

{

count=1;

}

}

void LedConfig(void)

{

/*Enable Clock for Port B. */

RCC->AHB2ENR |= (1U<<1);

/*Configure GPIOB_13 as general purpose output*/

GPIOB->MODER |= (1U<<26);

GPIOB->MODER &= ~(1U<<27);

}

void StartTimer6(void)

{

RCC->APB1ENR1 |= (1U<<4);

TIM6->PSC = 1000;

TIM6->ARR = 4000;

TIM6->EGR |= (1U<<0);

TIM6->DIER |= (1U<<0);

TIM6->CR1 |= (1U<<0);

NVIC_EnableIRQ(TIM6_IRQn);

}

void TIM6_IRQHandler(void)

{

if(TIM6->SR & (1U<<0))

{

GPIOB->ODR ^= (1U<<13);

TIM6->SR &= ~(1U<<0);

}

}

This discussion is locked. Please start a new topic to ask your question.
14 REPLIES 14
SSaiy.1
Associate III

Thanks @KnarfB as you said IRQ handler was different the actual one is TIM6_DACUNDER_IRQHandler. After I changed the handler name the code started working

KnarfB
Super User

Glad it works. To add some confusion: stm32l412xx.h (ARM CMSIS) and others contains a line

/* Aliases for __IRQHandler */
#define TIM6_IRQHandler                TIM6_DAC_IRQHandler

which covers that error up. But you don't seem to use that.

KnarfB

waclawek.jan
Super User

Nice catch, @KnarfB​ !

> TIM6_DACUNDER_IRQHandler

I've never seen handler name like this. As I've said above, I would like to know where that startup_stm32l412rbtx.s is from.

JW

when I tried the debug mode startup_stm32l412rbtx.s was autoloading because of the error, it was in the debug folder under projectname.elf -[arm/le]. I got the Handler name from this file.

0693W00000YAgnaQAD.png

What toolchain / version are you using?

KnarfB