STM32 I2C Multi-master problem
I'm seeing a problem which seems to be related to the one discussed here: https://community.st.com/s/question/0D50X00009XkgoYSAR/stm32-i2c-multimaster-hardware-bug
In my case though I'm not using DMA, I'm just using interrupt driven I2C but the symptom is the same:
When an MCU is addressed for a slave read at exactly the same moment it attempts to master a write transaction on the bus the collision is not detected as an arbitration loss, but the peripheral switches to slave transmission and performs that transaction, but then as soon as that is complete it starts the master transmission but with chaotic data values (uses the last TXDATA value that was loaded at the end of the slave transmission).
The closed bug referred to above mentioned that this was now a known bug in the I2C peripheral and that the errata sheets would be updated. However I can't find any mention of this behaviour in the errata sheets for the micros I'm using (an STM32F746 and STM32F071), both of which seem to display this behaviour.
Can you confirm whether this problem is expected to occur with these micros and whether there are any recommended workarounds please ?
Thanks,
Steve