2019-06-17 5:33 AM
Dear Members,
Is this function :
void max30100_FIFO_ReadBytes(uint8_t* Data)
{
//================READ FIFO DATA REGISTER======
buffer_tx[0] = 0x05;//FIFO DATA REGISTER //page 16 datasheet
//write one byte to MAX30100, 0xAE = Write to MAX30100, 0xAF = Read to MAX30100
HAL_I2C_Master_Transmit(&hi2c2, 0xAE, buffer_tx ,1, 100);
//HAL_Delay(5);
//Read from FIFO DATA Register
HAL_I2C_Master_Receive(&hi2c2, 0xAF, Data ,6, 10); //receive 6 bytes from MAX30100
}//end function Equal to :
void max30102_FIFO_ReadBytes(u8 Register_Address,u8* Data)
{
IIC_Start();
IIC_Send_Byte(max30102_WR_address | I2C_WR);
if (IIC_Wait_Ack() != 0)
{
goto cmd_fail;
}
IIC_Send_Byte((uint8_t)Register_Address);
if (IIC_Wait_Ack() != 0)
{
goto cmd_fail;
}
IIC_Start();
IIC_Send_Byte(max30102_WR_address | I2C_RD);
if (IIC_Wait_Ack() != 0)
{
goto cmd_fail;
}
Data[0] = IIC_Read_Byte(1);
Data[1] = IIC_Read_Byte(1);
Data[2] = IIC_Read_Byte(1);
Data[3] = IIC_Read_Byte(1);
Data[4] = IIC_Read_Byte(1);
Data[5] = IIC_Read_Byte(0);
IIC_Stop();
cmd_fail
IIC_Stop();?
Thanks