2015-05-20 2:08 AM
Hello,
I realize a project using stm3210e_eval,IDE: CooCoxDebugger: ST-Link V2When I'm debugging step-by-step, the cursor it's not linear !! and I don't understant Why ! for example: the cursor is at the line 170. when I click F10 or F11, the cursor don't pass at the line 171, but it back at the line 160 !!(''it's just an example to explain what I want to say'')Any help please ?thanks :) #stm32-debugging-st-link-problem2015-05-20 2:27 AM
I guess that you either turned on optimisation, or source code and executable aren't matching (out of sync).
Sorry, but I don't have/use Coocox.2015-05-20 2:56 AM
yes, you are right. I was turned on optimisation !
I've tried without optimisation, so the debugging problem is solvedThank you argentum ;)