2015-07-28 12:30 AM
Hi all,i am using STM32F0 and i want communication between 7E1 and 8N1.But STM32F0 haven't 7 bit communication option. How can i do this?
Thank you2015-07-28 12:47 AM
> Hi all,i am using STM32F0 and i want communication between 7E1 and 8N1.But STM32F0 haven't 7 bit communication option.
In the STM32 U(S)ARTs, parity bits are included in the data bits, so use the 8-bit option. JW2015-07-28 01:10 AM
2015-07-28 04:02 AM
My problem solved.I did as above and worked
2015-07-28 06:08 AM
You don't have to do anything when writing the transmit register, the STM32 adds the parity bit. When reading you want to mask either with & 0x7F, or & 0xFF, for the 7 and 8 bit data lengths.
For 7E1 you'd configure the USART in 8-bit mode with parity, for 8E1 you'd configure in 9-bit mode with parity.2024-08-28 05:49 AM
Hi all,i am using STM32C011F4U6 and i want communication between Uart1 _8N1 and Uart2_7E1.But STM32C0 haven't 7 bit communication option. How can i do this?
Thank you
2024-08-28 11:36 PM
@praveen2 Please also refer to this thread where you have asked the same question.