2014-04-01 11:56 PM
Hello everyone, I'm using STM32F100V8 and I configured TIM4 to generate a square wave (for uart sw). The TIM4 is so configured and should have the highest priority:
TIM_TimeBaseStructInit(&TIM_TimeBaseStructure); TIM_TimeBaseStructure.TIM_Period = 1; TIM_TimeBaseStructure.TIM_Prescaler = 405; TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure); TIM_ITConfig(TIM4, TIM_IT_Update , ENABLE); NVIC_PriorityGroupConfig(NVIC_PriorityGroup_1); NVIC_InitStructure.NVIC_IRQChannel = TIM4_IRQChannel; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); Inside the ISR of TIM4 i toggle a MCU line and my scope show me that the clock has a very high jitter; Could someone give me some suggestion to make te clock more stable ? Here attached an image from my scope acquired on a long time with infinite persistence time #stm32-clock-jitter-tim42014-04-02 12:47 AM
Don't toggle the output pin ''manually'' in the ISR. Rather, use one of the output compare channels and set it to change state in the ''future'' as needed.
A completely different approach may be to use the timer as trigger for DMA transferring from a prepared array in RAM to GPIO. JW2014-04-02 2:37 AM
Thanks for the reply. Could you please explain me why I can't toggle the pin manually inside the ISR ?
2014-04-02 3:00 AM
... to avoid the jitter caused by the zillions of factors causing variable latency of the ISR....
Mind, this is NOT a microcontroller. It's a SoC with relatively loosely (as far as timing goes) coupled modules. JW2014-04-02 6:42 AM
Could you please explain me why I can't toggle the pin manually inside the ISR ?
You can, but it's the stupid plan, the TIM peripheral is capable of toggling pins on a hard time line, or generating pulses, etc directly. If you do it in software you get to see all the latency and variability in the servicing.2014-05-05 1:28 PM
I have the similar problem. I am relying on the timer to provide constant timing for ADC sampling. SPI command is used to read the ADC. The CS pin negative edge starts the acquisition. I manually set and reset the CS pin in the interrupt routine, but the CS pin has high jitter. That adds lots of noise to my FFT plot. Is there a way to minimize the jitter? I am using STM32F415
2014-05-05 5:10 PM
You could presumably drive the CS pin as a TIM PWM signal, you could cause the pin to go low for a prescribed period, one into which you'd then perform your SPI transaction, starting it in the CCx interrupt
2014-05-06 12:20 PM
Sorry, I was not clear in my explanation. For the ADC that I use, both CS and SCLK must not have jitter. The ADC actually starts the acquisition at the fourth rising edge of SCLK. I understand your comment about using the PWM output as the CS signal, but that doesn't solve the jitter problem for SCLK.
2014-05-06 12:50 PM
Perhaps you can use a TIM triggered DMA into the SPI peripheral?
Other than that you might want to get the hardware sequencing handled in a CPLD?