cancel
Showing results for 
Search instead for 
Did you mean: 

Setting falling edge interrupt STM32F205RBt6

aamirali641989
Associate II
Posted on May 05, 2014 at 18:31

I want to set falling egde interrupt for PA15. I did below setting, but problem is interrupt occurs on both edges.

Pin is pulled up by 2.7K register to 5V.

I debug the code RTSR register has bit15 = 0, i.e rising edge disabled.

Didn't change RTSR & FTSR anywhere else in code.

void EXTI15_10_IRQHandler(void)

{

/* clear isr flag */

EXTI->PR = REG32_BIT_15;

// do something

}

void init()

{

/* make as input encoder I */    

    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);

  

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;

    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_15;

    GPIO_Init(GPIOA, &GPIO_InitStructure);

  

    SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOA, EXTI_PinSource15);

  

    EXTI->PR = REG32_BIT_15;

    EXTI->FTSR = (0xFF800000U & EXTI->FTSR) | REG32_BIT_15;

    EXTI->IMR = (0xFF800000U & EXTI->IMR) | REG32_BIT_15;

    

/* Enable and set EXTI Line2 Interrupt to the lowest priority */

    NVIC_InitStructure.NVIC_IRQChannel = EXTI15_10_IRQn;

    NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x00;

    NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x00;

    NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

    NVIC_Init(&NVIC_InitStructure);

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
chen
Associate II
Posted on May 06, 2014 at 17:22

Hi

''I want to set falling egde interrupt for PA15. I did below setting, but problem is interrupt occurs on both edges.''

Are you sure?

Could it be that you are getting contact 'bounce' - which give multiple IRQs - makes it look like IRQ on both edges.