2024-09-02 6:05 AM - edited 2024-09-02 6:05 AM
Hi,
I am trying to set up bootloader on my STM32G030, via usart.
When I enter it and send start command (0x7F) I do get ACK response(0x79). I cna read ID and protocol verions, but when I try do use "Go" command to start my application, it gets stuck.
What I am sending and responses I get from bootlaoder:
Send: 0x7F (start)
Response: 0x79
Send: 0x21 0xDE (go command)
Response: 0x79
Send: 0x0800004 0x04 (my application program is at address 0x08000000) (0x04 is length of address in bytes for checksum)
Response: nothing
I assume I am doing something wrong with checksum value, but I cant figure out what.
Solved! Go to Solution.
2024-09-02 6:14 AM
You can try the following sequence instead:
2024-09-02 6:14 AM
You can try the following sequence instead:
2024-09-02 6:25 AM - edited 2024-09-04 12:58 AM
Ok @liaifat85 , with this command procedure I get ACK after checksum. But my application is not starting after it. One of functions in my APP is that it repondes to a uart query (I send ID, it reponds with SYS). It know it works, because if I disable bootlaoder, and it goes straight in the APP, it works.
Might there be a problem with my address?
This is screen of STMcubeprogrammer:
After checking with debugger, after the bootlaoder "GO command" the program flow gets to main.c(set breakpoint at HAL_Init(); ), so there is some other problem with main APP not really working. Thank for your help.