2019-02-06 04:29 AM
Dear All,
I am going to use stm32f030f4 which has 16K flash & 4K SRAM. if I use STM32 bootloader , will Bootloader reduce available Flash/Ram or there is other reserved section for Bootloader i mean that i would like to save all flash/ram space for my application.
Best Regards,
Ahmed.
2019-02-06 04:34 AM
The RAM is a reusable resource when it comes to loaders.
If you write your own loader it will consume FLASH. The chip comes with a system loader in a separate ROM/OTP location that doesn't eat into your available FLASH space.
2019-02-06 04:37 AM
Thanks a lot for your reply.
what is the best document that i can read to use STM32 system loader
2019-02-06 05:01 AM
AN2606 is an overview. And there are others describing the protocol on different connections, USART might be most helpful, so AN3155.