cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 Bootloader & PC GUI Flash demonstrator

16-32micros
Associate III
Posted on July 03, 2008 at 20:40

STM32 Bootloader & PC GUI Flash demonstrator

14 REPLIES 14
16-32micros
Associate III
Posted on May 17, 2011 at 12:16

Dear all,

A new PC (Flash Loader) GUI demonstrator for the STM32 bootloader is available on this link :

http://www.st.com/stonline/products/support/micro/files/um0462.zip

;-) Enjoy it !

Regards,

STOne-32

nicolasfillon9
Associate
Posted on May 17, 2011 at 12:16

Hi,

I tried it on a B revision of chip on a Keil board and it works fine.

For those who have a Keil board you can use the attached .hex file.

BR,

Nicolas. :-D

sjo
Associate II
Posted on May 17, 2011 at 12:16

Had little success on rev A silicon - is it known to work?

Tried both IAR and Keil boards - currently have no rev B to try.

Cheers

sjo

wuguobing
Associate II
Posted on May 17, 2011 at 12:16

It doesn't work! The chip version is Rev B, Cable doesn't support hardware flow control. (The UART1 works fine.)

ivan239955_stm1_st
Associate II
Posted on May 17, 2011 at 12:16

Can somebody confirm that hardware flow control (RTS/CTS) is not required?

I tried to communicate with Flash loader demonstrator (v1.0) from serial port terminal (pretending to be STM32) and it seems to be happy just with 3 wires( Rx,Tx,GND).

However, when I replied to Get Command (as described AN2606, page 9/33) demonstrator reported error: ''cannot Get BL available commands''

Ivan

16-32micros
Associate III
Posted on May 17, 2011 at 12:16

Dear all,

I confirm that The flow control (RTS & CTS ) is not required. For revA and answering 'sjo' question we have some earlier versions of bootloader

(1.x) but now the stable version is ''2.0'' and this is available on all revB & Z devices. To version number is available by ''Get Version'' command and is shown in the Flash Loader demonstrator once the connection is done,

when you would like to select the target.

Regards, STOne-32

16-32micros
Associate III
Posted on May 17, 2011 at 12:16

Dear all,

I confirm that The flow control (RTS & CTS ) is not required. For revA and answering 'sjo' question we have some earlier versions of bootloader

(1.x) but now the stable version is ''2.0'' and this is available on all revB & Z devices. To version number is available by ''Get Version'' command and is shown in the Flash Loader demonstrator once the connection is done,

when you would like to select the target.

Regards, STOne-32

sjo
Associate II
Posted on May 17, 2011 at 12:16

Would it be possible to obtain a copy for revA silicon?

spencer_dot_oliver_at_anglia_dot_com

Regards

sjo

16-32micros
Associate III
Posted on May 17, 2011 at 12:16

Dear Oliver,

I recommand you to request your free STM32 new samples using the Free samples from our web site and to move to RevB/Z :-D and then Reworking it on you board (very easy if you have a good rework station). Regards,

STOne32 :-o