2019-08-13 3:11 AM
I am trying to use the built in boot-loader on my STM32F767. I wrote a simple app on my PC and I can get sensible answers from GET, GET VERSION, GET ID commands. But when I try to do a GO or a READ, the address (I have tries 0x00200000, 0x08000000 and 0 addresses) is rejected with a NAK.
Note that the READ or GO command itself is not rejected so it is not due to RDP or anything like that.
Any ideas why would be greatly appreciated.
So I got the STM Flash Loader Demo app to try that and it doesn't recognize my device.
If I try again I get a no response message unless I reset my board.
Any help on this would also be greatly appreciated.
Solved! Go to Solution.
2019-08-14 9:08 AM
Hello @KDuff.15 ,
The STM Flash Loader you are using does not support STM32F76x devices.
We recommend you to use the STM32CubeProgrammer software for programming STM32 products.
Best Regards
Imen
2019-08-13 3:16 AM
By the way, I am communicating using serial comms on USART1
2019-08-14 9:08 AM
Hello @KDuff.15 ,
The STM Flash Loader you are using does not support STM32F76x devices.
We recommend you to use the STM32CubeProgrammer software for programming STM32 products.
Best Regards
Imen