cancel
Showing results for 
Search instead for 
Did you mean: 

How to debug the Seeed Studio AI Assistant board using a STLink/V2 debugger

mtv
Associate III

Hello,

We have bought the new AI Assistant board from Seeed Studio and we need some help on how we can connect an external debugger.

We have two STLink/V2 debuggers, the plain and the ISOL version. However with the cables that they have we cannot connect any of them to the 8-pin debug port of the Seeed board.

We assume that the necessary pins are on the STM32 connector, but which are they? Additionally the picture of the STLink/V2 debugger in:

https://wiki.seeedstudio.com/ai_assistant_getting_started/#additional-documentation-of-the-application

does not correspond to the debugger we have. Is that a different board from the one we have?

https://www.st.com/en/development-tools/st-link-v2.html#overview

Thanks in advance

1 ACCEPTED SOLUTION

Accepted Solutions

First of all thanks for the reply. It is good to know the support options of Seeed Studio.

I wrote here because in the end of

https://wiki.seeedstudio.com/ai_assistant_getting_started/#resources

it clearly says that the product is supported by STMicroelectronics.

Also in the photo with the pinout next to ST-Link V3 it also has an image that says ST-Link V2.

However I found the solution searching the STMicroelectronics site. I found the technical note TN1235 "Overview of ST-LINK derivatives" and I understood that the photo in the Seeed site actually corresponds to the ST-Link V2-1 version that includes the Uart pins. The plain ST-Link V2 debuggers do not have the Uart pins. 

So finally with a Nucleo board as in the photo I managed to connect with the board. 

Thanks again

View solution in original post

2 REPLIES 2
Andrew Neil
Super User

@mtv wrote:

the new AI Assistant board from Seeed Studio


As it's a Seeed Studio board, you should be going to Seeed Studio for support:

https://aftersale.seeedstudio.com/home 

https://forum.seeedstudio.com/

https://discord.com/invite/QqMgVwHT3X

 

Particularly as it's a new product, you need to feeding back to them on needed improvements!

 


@mtv wrote:

We assume that the necessary pins are on the STM32 connector, but which are they?

That really is a question for Seeed Studio!

But the schematics are on the page you linked: 

https://wiki.seeedstudio.com/ai_assistant_getting_started/#resources

 


@mtv wrote:

the picture of the STLink/V2 debugger in:

https://wiki.seeedstudio.com/ai_assistant_getting_started/#additional-documentation-of-the-application

does not correspond to the debugger we have.


As it says in the picture, that's an ST-Link V3:

https://www.st.com/en/development-tools/stlink-v3set.html

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

First of all thanks for the reply. It is good to know the support options of Seeed Studio.

I wrote here because in the end of

https://wiki.seeedstudio.com/ai_assistant_getting_started/#resources

it clearly says that the product is supported by STMicroelectronics.

Also in the photo with the pinout next to ST-Link V3 it also has an image that says ST-Link V2.

However I found the solution searching the STMicroelectronics site. I found the technical note TN1235 "Overview of ST-LINK derivatives" and I understood that the photo in the Seeed site actually corresponds to the ST-Link V2-1 version that includes the Uart pins. The plain ST-Link V2 debuggers do not have the Uart pins. 

So finally with a Nucleo board as in the photo I managed to connect with the board. 

Thanks again