cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-STWINKT1B WiFi connection issue

Hi.. There
Recently i bought  STEVAL-STWINKT1B kit with the WiFi adapter. 
My motive is to connect the kit with the DSH-PREDMNT dashboard to run the FP-AI-PREDMNT2 demo

 

From my side, this is what i have done sofar

1. downloaded the FP-AI-PREDMNT2 firmware package

2. Installed the .bin file as it is what i found from the firmware package

3. Install the ST-BLE Sensor classic app with the phone and able to pair with the BLE

4. Made the account with the DSH-PREDMNT via default ST user credentials

5. Register the node via BLE APP with the DSH-PREDMNT dashboard

6. Added the WiFi credentials of one of my AP

However, everything goes well except WiFi connection!

Node never paired with the WiFi AP!

 

I never got the WiFi working with the default firmware!
I already got the JTAG debugger with the kit

To debug further more, i have forced the board in to the debug mode with the code!
but unfortunately, I'm not getting the debug logs at the serial terminal 

How do i activate the debug logs ?

pl. suggest

Thanks

Mahendra

1 REPLY 1
DDineshkumar
Associate II

Hello,

checking with you on the solution, I still face the same issue and wasn't able to connect to the dashboard even though the device was recognized by the st-ble and was added to the cloud interface I got struck with wi-fi connection. let me know if you have solved this issue which will help me!

Best Regards

Dinesh Kumar