cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-MKI117V1 Firmware sources

pat
Associate
Posted on March 25, 2014 at 18:22

I am developing an application using the MP34DT01 microphone and an STM32F4 microcontroller. I have an STEVAL-MKI117V1 evaluation board, which interfaces the microphone to an STM32F107. I would like to port the PDM input driver to the STM32F4.

Are the sources for the MKI117V1 eval board firmware available? If not, where do I find other example sources for PDM input? Thank you.
3 REPLIES 3
Amel NASRI
ST Employee
Posted on March 26, 2014 at 11:03

Isn't the

http://www.st.com/web/en/catalog/tools/PF258785

?

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

pat
Associate
Posted on April 03, 2014 at 03:07

Hi Mayla,

The APWorkbench software seems to be a client for audio processing that runs on a PC. I'm looking for the software that runs on the STM32 microcontroller itself.

Pat

Posted on April 03, 2014 at 14:03

Suggest you contact your local ST rep or FAE.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..