2012-11-01 9:29 AM
So does the whole family of STM32M0-STM32M4 have their own StdPeriphDriver offering? Under the advisement of my hardware guide, I am trying to test out the Freescale Freedom board after I have developed on the STM32F0 Discovery. I dont see anything on the Freescale side of the fence that comes close to providing the funtionality/ease of the std periph drivers st provides. Do NXP's cortex offering come with Std Periph Drivers like ST? Is Freescale the odd one out in not providing this? I am just a noob and I could setup my I/O on either the Freescale or ST using the below code: (obviously pinouts are different but would the functions/structure work?):
USART_InitTypeDef USART_InitStructure; /* SysTick end of count event each 1ms */ RCC_ClocksTypeDef RCC_Clocks; RCC_GetClocksFreq(&RCC_Clocks); SysTick_Config(RCC_Clocks.HCLK_Frequency / 1000); //IO Port Config /* GPIOC Periph clock enable */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE); // Watch Dog clock enable, config, enable RCC_APB1PeriphClockCmd(RCC_APB1Periph_WWDG, ENABLE); WWDG_SetPrescaler(WWDG_Prescaler_1); WWDG_SetWindowValue(0x7F); WWDG_Enable(0x7F); /* Configure PA0 and PA1 in output pushpull mode for LED1 and LED2 */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Configure PA4, PA5, PA6, PA7, PA8 in input pushpull for sensor selector switch */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7 | GPIO_Pin_8; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Configure PB8, PB9, PB10, PB11, PB12, PB13 in output pushpull mode for relay outputs */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10 | GPIO_Pin_11 | GPIO_Pin_12 | GPIO_Pin_13; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOB, &GPIO_InitStructure); /* Configure PC0, PC2, PC4, PC6, PC8 in output pushpull mode for 485 output enables DE */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_2 | GPIO_Pin_4 | GPIO_Pin_6 | GPIO_Pin_8; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOC, &GPIO_InitStructure); /* Configure PC1, PC3, PC5, PC7, PC9 in output pushpull mode for 485 input enables RE'*/ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1 | GPIO_Pin_3 | GPIO_Pin_5 | GPIO_Pin_7 | GPIO_Pin_9; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOC, &GPIO_InitStructure); //End of IO Port Config