cancel
Showing results for 
Search instead for 
Did you mean: 

Std peripheral library manual PDF? CAN examples?

alexalex9
Associate II
Posted on August 09, 2010 at 21:30

Std peripheral library manual PDF? CAN examples?

3 REPLIES 3
Posted on May 17, 2011 at 14:01

''Is there a PDF format manual for the V3 std peripheral library, like UM0427 was for the V2?''

 

No, there isn't.

:(

This is a Really Bad Thing, IMO.

See:

https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/DispForm.aspx?ID=10446&RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM CortexM3 STM32/UM0427 - firmware library - is missing!&Source=https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM%2520CortexM3%2520STM32/Flat.aspx?RootFolder%3Dhttps%253a%252f%252fmy%252est%252ecom%252fpublic%252fSTe2ecommunities%252fmcu%252fLists%252fARM%2520CortexM3%2520STM32%252fUM0427%2520%252d%2520firmware%2520library%2520%252d%2520is%2520missing%2521%26FolderCTID%3D0x01200200770978C69A1141439FE559EB459D758000626BE2B829C32145B9EB5739142DC17E%26currentviews%3D593

alexalex9
Associate II
Posted on May 17, 2011 at 14:01

Ouch.  My opinion too.  I should mention to ST that the existence of a documented API was a factor in my jumping to the STM32, and that it has made learning the part much easier.

Posted on May 17, 2011 at 14:01

''the existence of a documented API was a factor''

To be fair, the API is documented - it's just that the documentation is no longer in the form of a PDF!