2013-06-18 7:22 AM
Hello,
I'm new user. I read many documents, but I havedoubts
. I'm working with uVision. My question is: is it possible load flash memory by mini usb? If yes, How I can configure debug option in uVision? THANKS #stm32f4-discovery-usb2013-06-18 9:16 AM
USB connector CN1 provides connection the ST-LINK (SWD Debugger) on the board.
You will need to make sure the ST-LINK driver is installed (\Keil\ARM\STLink) In Keil, depending on the ST-Link firmware you'd need to pick ''ST-Link (Deprecated Version) or ''ST-Link Debugger'', you also need to ensure you pick ''SWD'' mode in the settings, as ''JTAG'' is not supported.