cancel
Showing results for 
Search instead for 
Did you mean: 

ST7789

farhad1365
Associate

According to the datasheet, what is the maximum speed of the ST7789 for the SPI protocol? If we use an LCD with the ST7789 driver and connect it via the SPI protocol to a microcontroller, would we get higher speed with the STM32G0B0CET6 microcontroller or the STM32H562RIT6 microcontroller? Or does it not make a difference due to the speed limitation of the ST7789 driver?

1 REPLY 1

It's a Sitronix not an STMicro part.

There's perhaps timing parameters providing an upper ceiling

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..