2014-08-07 9:36 AM
Hi,
I'm newbie to STM32. I use Keil to program my Nucleo F401RE board. The program simply change the LED (PA05) blinking rate when user button (PC13) is pressed. I used HAL_SYSTICK_Callback() and HAL_GPIO_EXTI_Callback(). It works fine as expected. However, I notice that pin PC10 keep swinging low high every 2 seconds although it was not configured to do so. I removed all the code until only 3 lines like below but it still swings:int main(){ HAL_Init();__GPIOC_CLK_ENABLE(); while(1){}}What's the problem with the pin?Thanks