Posted on October 23, 2012 at 15:59I got an error when I tried to connect to the ST-LINK/V2, with V 2.2. Someone else suggested CrossWorks, as a cheap compiler. Leon
Posted on October 23, 2012 at 15:09I'm using the Rowley tools with the STM32F4 Discovery, they work very well and the IDE is the nicest one I've used - far better than Eclipse. I had to use the unreleased V 2.3, which is still being developed. Leon