Posted on September 07, 2017 at 17:55HiI'm using a STM32F103ZEI'm trying to configure DMA1 with ADC1 Channels 12 & 16.The code below works i.e. when the DMA flags the DMA_Buffer contains 800 samples, 400 for Channel_12 and 400 for Channel_16Howe...
Posted on October 30, 2014 at 16:54Hi Is there an example code or library for the stm32f10x that does AES128 encryption\decryption with CBC cipher mode. thanksLiam
Posted on September 08, 2017 at 11:53 I'm already using ADC2 for SD. For now I'm going to just going to Disable the DMA for Channel 12, ReConfigure and take a reading on Channel 16 (takes ~0.4 ms) ReConfigure DMA ADC1 for Channel 12 I o...
Posted on July 01, 2013 at 13:41Removed drivers, downloaded and installed latest drivers, and now the ST-LINK CLI.exe works on my 64 Bit Windows 7, so all good again
Posted on June 26, 2013 at 15:11On Windows 64bit I can get the STM32 ST-LINK Utility.exe to work.However as Phil said in first post I can't get the ST-LINK CLI.exe to work Is it compatible with Windows 64 Bit?