2017-06-05 11:42 PM
Hello,,
I need to write (or modify) a new External flash loader for StLink utility.
I'm using a STM32F475RCT6 with a N25Q128A13EF840E Quad Spi Flash.It's seems to be very similar to the example given with StLink Utility (STM32L476G_EVAL\Examples\QSPI\N25Q256A_STM32L476G-EVAL).
For me, the first step is to compile the software given as example.Compiler : IAR
Version : 7.70.1After renaming the elf file in stldr and copying it in the directory C:\Program Files\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Utility\ExternalLoader\, the external loader is seen by StLink Utility.
But :
- the external loader has no name - the 2 features available are Sector Erase and Program - no sector description is available for sector erase - Erasing, Programming or reading the externam flash is impossibleWhat are the good conditions (Define, ...) for compiling the project given as example?
Thanks
2017-06-15 08:40 PM
Hi, I have the same issue.
2017-09-06 04:28 AM
Try it in IAR 7.4 version.
2017-09-26 04:28 AM
Hi there!
You were talking about the following folder?:
ExternalLoader\\N25Q256A_STM32L476G-EVAL_Cube\Projects\STM32L476G_EVAL\Examples\QSPI\N25Q256A_STM32L476G-EVAL\
We can't find this folder anywhere.
For our project we are also searching for this example. Is it possible to send us a zipped file with that template?
Best regards,
2017-09-26 03:37 PM
C:\Program Files (x86)\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Utility\ExternalLoader\N25Q256A_STM32L476G-EVAL\Sources\Loader_Files\Loader_Src.c
from the v3.9.0 or v4.x.x installs as I recall
________________ Attachments : N25Q256A_STM32L476G-EVAL.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyMY&d=%2Fa%2F0X0000000b79%2FiAULu2h2wDVQVOFkbP9i78kyuDQyZwL5QaP4iskN57o&asPdf=false