ST-LINK Utility external NOR-FLASH programming
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-08-11 3:18 AM
Hello
. I have ARM MCU boardSTM32F407
(Schematic: http://www.keil.com/mcbstm32f200/mcbstm32f200-schematics.pdf )
It is connected to
NOR FLASH ( http://www.jameco.com/Jameco/Products/ProdDS/1472780.pdf ) who wantto program
in ST
-Link
Utility.
I have a problem with writing * .stldr for ST
LINK.
Please help with configuring ''
Dev_Info.c
''
Is this configuration
good
: struct StorageInfo const StorageInfo = { ''KEIL_BOARD'', NOR_FLASH, 0x60000000, 0x00400000, 0x00000002, 0xFF, // Specify Size and Address of Sectors (view example below) 0x00000008, 0x00001000, 0x0000007F, 0x00008000, 0x00000000, 0x00000000, }; #stm32 #external-memory #nor-flash- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-08-15 10:24 AM
Does anyone wrote code for programming the external memory for ST-Link
?- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-08-15 11:47 AM
Does anyone wrote code for programming the external memory for ST-Link?
Yes, are you in the market for such?Your data structure really doesn't seem to accurately describe the M29W640FT NOR memory. Did you review the cited data sheet?Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-08-15 12:41 PM
A more detailed
description of the structure
: struct StorageInfo const StorageInfo = { ''KEIL_BOARD,V1.0'', // Device Name + version number NOR_FLASH, // Device Type 0x60000000, // Device Start Address 0x00400000, // Device Size in Bytes (16MBytes/128Mbits) 0x00000008, // Programming Page Size 16Bytes 0xFF, // Initial Content of Erased Memory // Specify Size and Address of Sectors 0x00000008, 0x00001000, // 8 Sectors of 8KBytes 0x0000007F, 0x00008000, // 127 Sector of 64KBytes 0x00000000, 0x00000000, // End };- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-08-15 1:34 PM
Half the numbers and comments are wrong.
Your FSMC initialization would also need to be 100% correct to stand any chance of working.I would suggest you code NOR Writing into your current application/template, and prove and test that outside of the ST framework. Once you have that working properly you'll be in a position to port it into the loader format.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-08-15 10:31 PM
Can you help with structure?
FSMC configuration is correct. Communication memory is tested. Tested function FSMC_NOR_Test(void), gives correct resultsvoid BOARD_NOR_Init(void)
{
FSMC_NORSRAM_TimingTypeDef NorTiming;
FSMC_NORSRAM_InitTypeDef NorInit;
NorInit.NSBank = FSMC_NORSRAM_BANK1;
NorInit.DataAddressMux = FSMC_DATA_ADDRESS_MUX_DISABLE;
NorInit.MemoryType = FSMC_MEMORY_TYPE_NOR;
NorInit.MemoryDataWidth = FSMC_NORSRAM_MEM_BUS_WIDTH_16;
NorInit.BurstAccessMode = FSMC_BURST_ACCESS_MODE_DISABLE;
NorInit.WaitSignalPolarity = FSMC_WAIT_SIGNAL_POLARITY_LOW;
NorInit.WrapMode = FSMC_WRAP_MODE_DISABLE;
NorInit.WaitSignalActive = FSMC_WAIT_TIMING_BEFORE_WS;
NorInit.WriteOperation = FSMC_WRITE_OPERATION_ENABLE;
NorInit.WaitSignal = FSMC_WAIT_SIGNAL_DISABLE;
NorInit.ExtendedMode = FSMC_EXTENDED_MODE_DISABLE;
NorInit.AsynchronousWait = FSMC_ASYNCHRONOUS_WAIT_DISABLE;
NorInit.WriteBurst = FSMC_WRITE_BURST_DISABLE;
/* Timing */
NorTiming.AddressSetupTime = 6;
NorTiming.AddressHoldTime = 15;
NorTiming.DataSetupTime = 6;
NorTiming.BusTurnAroundDuration = 15;
NorTiming.CLKDivision = 2;
NorTiming.DataLatency = 17;
NorTiming.AccessMode = FSMC_ACCESS_MODE_B;
/* Initialize NOR control Interface */
FMC_NORSRAM_Init(FSMC_NORSRAM_DEVICE, &NorInit);
/* Initialize NOR timing Interface */
FMC_NORSRAM_Timing_Init(FSMC_NORSRAM_DEVICE, &NorTiming, NorInit.NSBank);
/* Initialize NOR extended mode timing Interface */
FMC_NORSRAM_Extended_Timing_Init(FSMC_NORSRAM_EXTENDED_DEVICE, &NorTiming, NorInit.NSBank, NorInit.ExtendedMode);
/* Enable the NORSRAM device */
__FMC_NORSRAM_ENABLE(FSMC_NORSRAM_DEVICE, NorInit.NSBank);
/* SRAM controller initialization */
BOARD_GPIO_NOR_Init();
}
void FSMC_NOR_Test(void)
{
uint16_t index;
HAL_NOR_StatusTypeDef flag_erase = HAL_NOR_STATUS_ERROR;
flag_erase = FSMC_NOR_EraseChip();
FSMC_NOR_EraseBlock(WRITE_READ_ADDR);
for (index = 0; index < BUFFER_SIZEE; index++ )
{
TxBuffer[index] = index + 121;
}
FSMC_NOR_WriteBuffer(TxBuffer, WRITE_READ_ADDR, BUFFER_SIZEE);
/* Read data from FSMC NOR memory */
FSMC_NOR_ReadBuffer(RxBuffer, WRITE_READ_ADDR, BUFFER_SIZEE);
if( memcmp( (char*)TxBuffer, (char*)RxBuffer, BUFFER_SIZEE ) == 0 )
{
HAL_GPIO_WritePin(LED6_GPIO_PORT,LED6_PIN, GPIO_PIN_SET); // Nor Flash is OK
}
else
{
HAL_GPIO_WritePin(LED6_GPIO_PORT,LED6_PIN, GPIO_PIN_RESET); // Nor Flash is error
}
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-08-17 3:23 AM
I'm still
double-check
code.Code is
well written.
The structure is not good?
What's wrong?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-08-17 5:19 AM
The structure is not good? What's wrong?
Like I told you, half the numbers are wrong, this should correctly describe the partstruct StorageInfo const StorageInfo = {
''KEIL_MCBSTM32F400_M29W640FT/V100'', // Device Name + version number
NOR_FLASH, // Device Type
0x60000000, // Device Start Address
0x00800000, // Device Size in Bytes (8MBytes/64Mbits)
0x00000008, // Programming Page Size 8Bytes (Nominal)
0xFF, // Initial Content of Erased Memory
// Specify Size and Address of Sectors
0x00000008, 0x00002000, // 8 Sectors of 8KBytes
0x0000007F, 0x00010000, // 127 Sector of 64KBytes
0x00000000, 0x00000000, // End
};
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-08-17 5:54 AM
Can a more detailed
description of the structure
? Board MCBSTM32F400have M29W640FB (not M29W640FT )
0x60000000
- start address is correct0x00800000
- memory pin 47 (BYTE#),connected to
VCC,then
- data 16bit - memory size 4Mb ???0x00000008 - Programming Page, good size pages ???
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-08-17 6:29 AM
It is a 64Mb device whether it is accessed as bytes or words. There are 8MB in a 64Mb device. The CPU has a byte addressable address space, and these bytes don't change size if the downstream bus needs to handle 8, 16 or 32-bit widths to the memory array.
Mb megabit MB megabyte 8x1024x1024 = 8388608 = 0x800000 4096 = 0x1000 8192 = 0x2000 65536 = 0x10000Up vote any posts that you find helpful, it shows what's working..