cancel
Showing results for 
Search instead for 
Did you mean: 

st-link v2 supports stm32wl5moch ?

avinashkumar
Associate

dose st-link v2 is not supported in stm32wl5moch

2 REPLIES 2
STTwo-32
ST Employee

Hello @avinashkumar and welcome to the ST Community.

Could you please upload a photo of your ST-LINK V2. The  ST-LINK should work with any STM32 MCU/Module.

Best Regards,

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Andrew Neil
Super User

An ST-Link should support any STM23 with SWD or JTAG - which includes stm32wl5moch.

 

Do you have a specific problem with an ST-Link V2 and stm32wl5moch ?

If so, please give full details - see: How to write your question to maximize your chances to find a solution.

 

Be sure that you have a genuine ST-Link:

How to recognize a genuine ST-LINK/V2 versus a cloned one

That'll be why @STTwo-32 is asking for a photo.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.