2018-11-20 12:55 AM
Hi all,
I have a problem to show float numbers via sprintf, I'm working with STM32F334
I did a program to print via serial the voltage read from ADC, in float format like %4.2f, the problem is that the first time the sprintf generate a valid string with decimal separator, but the next iterations not.
I followed the tip recommended for @Hae Ryon Jung in this entry of forum, but I didn't get a good result
Any idea?
This is the code:
adcVal = HAL_ADC_GetValue(&hadc1);
adcRes = adcVal*3.3/4096;
sprintf(buffTmp, "[%d]ADC %d %4.2f V\n\r", (int) counter, (int)adcVal, adcRes);This is the output:
[0]ADC 2531 2.04 V
[1]ADC 2493 204 V
[2]ADC 2495 204 VThanks for your support
Regards
Jordi
2018-11-20 1:35 AM
Use printo (...), https://bitbucket.org/AVI-crak/sprint.
Recognizes: "text", double, float, uint (8-16-32-64) _t, int (8-16-32-64) _t in any sequence.
The magic "[% d] ADC% d% 4.2f V \ n \ r" is not required.
printo ("ADC", counter, ((float) adcVal / 1024.0f), "V \n");
2018-11-20 3:15 AM
Hi AVI-crack,
thanks for your feedback.
But, I think (and hope) that the same sprintf integrated in Atollic has to support it, I don't want to add more libraries (keep small footprint, and manteinable code)
Regards
Jordi
2018-11-20 4:00 AM
They have different weight, printo is much lighter.
2018-11-20 3:26 PM
remove nano.specs from your linker options
2018-11-20 11:02 PM
Hi John,
thanks for your feedback.
But it doesn't work.
I remove nano.spec from linker and I get the same, even worst result. The text area increase aprox 3KB, and RAM 1KB, and output is still wrong .
Regards
Jordi
2018-11-21 1:49 AM
Jordi Becares
Delete is not required. The built-in libraries contain optimized zero-level code for the ARM core, such as hardware multiplication, division, floating point operations, and so on. The part of the library that is not used is removed from the final layout of the firmware. It is enough not to use heavy functions. (find and delete any use).
But the information on ram / rom size increase looks strange. I had the opposite.
Use optimization level 02 or higher.
2018-12-05 12:23 AM
Hi,
I'm using Optimize for size(-Os).
I dont' fix the error yet. The sprintf of float number is not working well.
Any idea?
Regards
Jordi
2018-12-07 2:15 PM
I can not repeat the mistake.
I always get the correct floating point printing for sprintf (), printf (), and my printo ().
In your case, there is a magic change in the type of the variable, possibly outside the visible code.
2018-12-09 11:34 PM
What uC are you using?
Please, could you attach your project? So, I will check in my board
Thanks
Jordi