cancel
Showing results for 
Search instead for 
Did you mean: 

SPICE Model for STM32L4 OpAmp ?

ValereAq
Associate II

We need to perform some SPICE (LTSpice most likely) simulation of analog circuitry using the STM32L4 OpAmp (TQFP package not BGA).

I can only find this IBIS model, which will not help me much for this analog case, and not the SPICE model, which would help a lot.

Where could I find the Spise Model of the STM32L4 OpAmp when used as "standalone" will all the IO pins output on MCU external pins (both in "normal mode" and "low power mode") ? Would it be possible to get it or to get support to create it ?

Thanks.

--
More than a few hundred uA it's way too much... let's keep it under 10 uA or so please...
1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Bonjour @ValereAq et Bienvenue :smiling_face_with_smiling_eyes:

In fact, the Spice Model of the STM32L4 OPAMP is not available. But you could use standard OPAMP model just setting its parameters as given in datasheet of your MCU (for example the table 82 of the DS12469). The parameters depend on the settings you choose for the OPAMP. Then you can use it for simulation.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
STTwo-32
ST Employee

Bonjour @ValereAq et Bienvenue :smiling_face_with_smiling_eyes:

In fact, the Spice Model of the STM32L4 OPAMP is not available. But you could use standard OPAMP model just setting its parameters as given in datasheet of your MCU (for example the table 82 of the DS12469). The parameters depend on the settings you choose for the OPAMP. Then you can use it for simulation.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thanks,

I will test like this creating a model with the datasheet specifications.

I was interested to perform phase stability simulation also trying to introduce  temperature shift, this is why I was searching if a more advance model were available.

Best regards.

--
More than a few hundred uA it's way too much... let's keep it under 10 uA or so please...