SPI3 in stm32f10x problem
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-03-01 11:53 PM
Hi,
Sorry I take the forum user's time for my simple questions.
Here is my code for spi3 in stm32f10x for PB3 and PB4 output/input.
SPI_InitTypeDef SPI_INS;
GPIO_InitTypeDef GPIOS RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB,ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI3,ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO,ENABLE); GPIO_PinRemapConfig(GPIO_Remap_SPI3,DISABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4| GPIO_Pin_5|GPIO_Pin_3; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOB, &GPIO_InitStructure); SPI_INS.SPI_Direction =SPI_Direction_2Lines_FullDuplex; SPI_INS.SPI_Mode = SPI_Mode_Master; SPI_INS.SPI_DataSize = SPI_DataSize_8b; SPI_INS.SPI_CPOL = SPI_CPOL_High; SPI_INS.SPI_CPHA = SPI_CPHA_1Edge; SPI_INS.SPI_NSS = SPI_NSS_Soft; SPI_INS.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_128; SPI_INS.SPI_FirstBit = SPI_FirstBit_MSB; SPI_INS.SPI_CRCPolynomial = 7; SPI_Init(SPI3, &SPI_InitStructure); SPI_Cmd(SPI3, ENABLE); SPI_SSOutputCmd(SPI3,DISABLE); SPI_I2S_ITConfig(SPI3,SPI_I2S_IT_RXNE,ENABLE);However I can't see any clock signal in PB3 pin when I start sending ff value with SPI_I2S_SendData(SPI3, 0xff); function.
in STM32cubemx something is more strange:
According to datasheet we understand that for SPI3 without any remap PORT B can play SPI role.
However in STM32cubemx when I enable SPI3 and see it's configuration it just enables port c SPI section and it doesn't config anything such as remap.In addition when I change SPI3 for Port B it only change clock source.
STM32CubeMX output:
(REMAP)(PORTC) GPIO configuration
static void MX_GPIO_Init(void)
{/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();}
and (without REMAP)(PORTB) GPIO configuration
static void MX_GPIO_Init(void)
{/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOB_CLK_ENABLE();}
Solved! Go to Solution.
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-03-07 12:30 PM
Perhaps the Remap code is elsewhere, like where it actually configures the pins, or the SPI peripheral.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-03-07 12:30 PM
Perhaps the Remap code is elsewhere, like where it actually configures the pins, or the SPI peripheral.
Up vote any posts that you find helpful, it shows what's working..