2012-12-06 6:28 AM
Hi all,
To read or write a register of ADS1298 I need to write 3 byte on SPI bus and I need some delay between every byte. Based on the discovery example I write the following read and write routine: uint8_t ADS1298ReadRegister(uint8_t ChipNumber, uint8_t Register){ uint8_t RxRegister; // SPI_Cmd(SPI1,ENABLE); if (ChipNumber == ADS1298_1) SPI1_CS1_LOW(); else SPI1_CS2_LOW(); // while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET); SPI_I2S_SendData(SPI1, (uint16_t)(ADS1298_CMD_RREG + Register)); // SPI_I2S_SendData(SPI1, 0x0000); while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET); SPI_I2S_ReceiveData(SPI1); while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET); for (int i=0;i<200;i++); SPI_I2S_SendData(SPI1, 0x0a); while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET); SPI_I2S_ReceiveData(SPI1); while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET); for (int i=0;i<200;i++); SPI_I2S_SendData(SPI1, 0x05); while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET); RxRegister = SPI_I2S_ReceiveData(SPI1); // while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET); // while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET); if (ChipNumber == ADS1298_1) SPI1_CS1_HIGH(); else SPI1_CS2_HIGH(); // SPI_Cmd(SPI1,DISABLE); return RxRegister; } uint8_t ADS1298WriteRegister(uint8_t myChipNumber, uint8_t Register, uint16_t Value,uint8_t verify){ uint8_t RxRegister; // SPI_Cmd(SPI1,ENABLE); if (myChipNumber == ADS1298_1) SPI1_CS1_LOW(); else SPI1_CS2_LOW(); // while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET); SPI_I2S_SendData(SPI1, (uint16_t)(ADS1298_CMD_WREG + Register)); // SPI_I2S_SendData(SPI1, 0x0000); while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET); SPI_I2S_ReceiveData(SPI1); while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET); for (int i=0;i<200;i++); SPI_I2S_SendData(SPI1, 0x0a); while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET); SPI_I2S_ReceiveData(SPI1); while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET); for (int i=0;i<200;i++); SPI_I2S_SendData(SPI1, Value); while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET); SPI_I2S_ReceiveData(SPI1); // while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET); // while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_BSY) != RESET); if (myChipNumber == ADS1298_1) SPI1_CS1_HIGH(); else SPI1_CS2_HIGH(); // SPI_Cmd(SPI1,DISABLE); for (int i=0;i<300;i++); // SPI_Cmd(SPI1,ENABLE); if (verify){ RxRegister = ADS1298ReadRegister(myChipNumber,Register); if (RxRegister == Value) return 0; else return 1; } return 0; } When I tested these two routine reading and writing the ADS1298 register I found that sometimes I have 16 clock cicle on the bus while I setting the SPI size at 8 bit (see Below) // ADS1298 CPOL bit is a '0' and its CPHA bit is a '1'. SPI_I2S_DeInit(SPI1); SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; // SPI_InitStructure.SPI_DataSize = SPI_DataSize_16b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low; SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_8; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; //SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_LSB; // SPI_InitStructure.SPI_CRCPolynomial = 0; SPI_InitStructure.SPI_CRCPolynomial = 7; SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_Init(SPI1, &SPI_InitStructure); Could someone help my to find the root cause of this wrong SPI behaviour? I sperimentally found that if I set the SPI first bit with LSB the problem disappear. Thanks Luca Below the oscilloscope image. On ch1 there is the CS while on ch2 there is the SPI Clock Write Register correct Write problem READ CORRECT READ PROBLEM2012-12-06 6:34 AM
Sorry I tried to attach the oscilloscope images but while in the inserting message the image are present when I show the post the images disappear...
2012-12-06 6:38 AM