cancel
Showing results for 
Search instead for 
Did you mean: 

SPI Slave - Data received with errors

friquero
Associate II
Posted on April 17, 2013 at 00:35

I'm working with two STM32L151 communicating them via SPI port A-Master and B-Slave. I can only receive data correctly in B-Slave if I switch off transmission but I want full duplex in master and in slave. I can't either make the examples work properly. Has anybody had the same problem ?? I have attach the source code if someone wants to test it.  

#forum-says-no #stm32l151-spi-slave
2 REPLIES 2
friquero
Associate II
Posted on April 22, 2013 at 22:32

I would like to know if someone has had the same problem?. Any idea why is not working properly ?

Posted on April 23, 2013 at 04:20

I have attach the source code if someone wants to test it.  

Unfortunately your project is incomplete, using hardware and interfacing which isn't described. This would tend to limit the audience you're likely to attract, and the pool is already pretty shallow.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..