cancel
Showing results for 
Search instead for 
Did you mean: 

SPI Signal Shape Issue

AE104
Senior

Hello,

I am try to control an external DAC system with the SPI interface. The clock signal shape looks like the attached file. I didn't figure out the meaning of the signal. Yellow is the clock signal and the blue is CS signal.0693W00000aJE10QAG.jpg

24 REPLIES 24
AE104
Senior

This is the latest measurement that I have.

AScha.3
Chief III

again sample rate much too low. 500 ks - how you do this ?

+

or do you make "SINGLE" shot and then turn around the timing? this could make such pictures.

show a measurement without any change or "adjustment" after the single shot.

If you feel a post has answered your question, please click "Accept as Solution".
AScha.3
Chief III

When your question is answered, please mark this topic as answered by choosing Select as Best for the preferred answer, as also explained here. This will help other users find that answer faster.

If you feel a post has answered your question, please click "Accept as Solution".

Sorry for late reply. Honestly, I don't know, for example now the sampling rate of the oscilloscope is 1 GSa/s.

You're right. I captured only this zoom in figure. Before zoomed in, it was square wave.

AE104
Senior

Sure, thank you @AScha.3​ , @Community member​ , and @Community member​ for your comments!