cancel
Showing results for 
Search instead for 
Did you mean: 

SPI Signal Shape Issue

AE104
Senior

Hello,

I am try to control an external DAC system with the SPI interface. The clock signal shape looks like the attached file. I didn't figure out the meaning of the signal. Yellow is the clock signal and the blue is CS signal.0693W00000aJE10QAG.jpg

24 REPLIES 24
AE104
Senior

I pressed the CLEAR and AUTO, now the sampling rate is 250 MSa/s with 300k pts.

The bandwidth of the isolator is 25 Mbps

Is the signal on the STM32 side clean? Not ringing?

If the traces are short, ease back the slew-rate via SPEEDR settings.

What speed is your SPI clocking at?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
AE104
Senior

Now the updated signals look like the attached figures (the isolator removed).

The SPI Baudrate 10.5 Mbits/s.0693W00000aJEfjQAG.jpg

AE104
Senior
 
AScha.3
Chief III

better.

probe still at x1 ! you cannot test cmos connections at > 10MHz with x1 probe setting.

set x10 at probe switch and in scope menu.

If you feel a post has answered your question, please click "Accept as Solution".
AE104
Senior

I set the 10x both the probe and settings in the oscilloscope.

0693W00000aJElwQAG.jpg0693W00000aJEm1QAG.jpg

AScha.3
Chief III

x10 probe setting needs adjustment - did you adjust ?

+ BW limit 20 M is set.

do you make some game here ? who is the biggest idiot ? or what ?

sorry.

want help - or play game ?

If you feel a post has answered your question, please click "Accept as Solution".
AE104
Senior

No game. What adjustment do I need?

AScha.3
Chief III

bw limit off.

and adjust probes - i hope you know how to do.

If you feel a post has answered your question, please click "Accept as Solution".
AE104
Senior

Yes I did it.