Skip to main content
Simon Schmid
Associate
August 25, 2017
Question

SPI RXONLY with DMA possible?

Posted on August 25, 2017 at 15:30

I'm planning to use a STM32L432KC to read 18-bit transmission from an external slave device. It seems the RXONLY master mode is a perfect match for this since it is outputting a continous SPI clock. I could set the transfer size to 9bits and fill a DMA buffer with samples and stitch them together to 18-bits in the DMA's buffer full interrupt. (I intend to collect a few hundred sample in the buffer)

The datasheet is however a bit unclear, it states that

Each direction has its own FIFO called TXFIFO and RXFIFO. These FIFOs are used in all SPI modes except for receiver-only mode (slave or master)

Which means, there is no FIFO for RXONLY mode? Further, the datasheet says the RXNE event is dependent on the FIFO.

The RXNE flag is set depending on the FRXTH bit value in the SPIx_CR2 register:

    � If FRXTH is set, RXNE goes high and stays high until the RXFIFO level is greater or equal to 1/4 (8-bit).

    � If FRXTH is cleared, RXNE goes high and stays high until the RXFIFO level is greater than or equal to

      1/2 (16-bit). An interrupt can be generated if the RXNEIE bit in the SPIx_CR2 register is set.

To use the DMA I need the RXNE flag though:

RXDMAEN: Rx buffer DMA enable

When this bit is set, a DMA request is generated whenever the RXNE flag is set.

Is it impossible to use DMA with RXONLY? 

#stm32-spi-rxonly #stm32l4-spi #stm32l432kc #dma #stm32l4 #spi
This topic has been closed for replies.

2 replies

ST Technical Moderator
September 8, 2017
Posted on September 08, 2017 at 18:19

Hi,

DMA can be used for

RXONLY. 

When the SPI is used only to receive data, it is possible to enable only the SPI Rx DMA channel.

Have a look to the reference manual in the section 'Serial peripheral interface (SPI)' exactly in the 'Communication using DMA (direct memory addressing)' 

Best Regards

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Senior
September 14, 2017
Posted on September 14, 2017 at 12:50

At least in my situation it won't work with DMA.  The first data read in always wrong, and all data shifted backward one element. My tool chain is STM32F429, with STM32Cube 4.22.0 and STM32Cube FW_F4 V1.16.0, and the HAL function used is 'HAL_SPI_Receive_DMA()'.