cancel
Showing results for 
Search instead for 
Did you mean: 

RM0390 typo

zebra_scopper76
Associate

Documentation: RM0390
Revision: Rev 7, June 2025

Section 26.3.2 Page number 830:

Under Simplex communications, it says the RXONLY bit is in the SPI_CR2 register but the register map confirms RXONLY bit is in the SPI_CR1 register.

1 ACCEPTED SOLUTION

Accepted Solutions
Issamos
Lead III

Hello @zebra_scopper76 

This is a minor typo on the Simplex communication paragraph. I think @Imen.D you may help reporting this issue to be rectified on the future.

Best Regards.

II

View solution in original post

2 REPLIES 2
Issamos
Lead III

Hello @zebra_scopper76 

This is a minor typo on the Simplex communication paragraph. I think @Imen.D you may help reporting this issue to be rectified on the future.

Best Regards.

II

Imen.D
ST Employee

Hello @zebra_scopper76 , @Issamos 

Thank you for having reported this.

An internal ticket number 219990 is submitted to fix this typo in the coming release of RM0390.
(PS: Ticket number 219990 is an internal tracking number and is only for reference. It is not accessible or usable by customers).

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen